Other Parts Discussed in Thread: TPS25750
HI
BQ25792 There is something strange in operation, so please inquire.
I am using a SHIP FET configuration.
However, if the SHIP FET is used and the BATTERY is connected, the SDRV voltage is output abnormally.
Also, when I connect the adapter, it doesn't recognize it.
However, when the USB type c adapter is connected, If I remove the battery and plug it back in, it works normally.
The SDRV pin voltage is also output normally.
Can you tell me why?
<Abnormal SDRV PIN Voltage Output>
<Normal SDRV PIN Voltage Output>