Other Parts Discussed in Thread: EV2400
Hi
The customer feedback that bq40z50-r2 crashes, They did not do any test, but this happened when it was placed.
When will the BQ40Z50-R2 crash,
Waiting for your reply.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The customer feedback that bq40z50-r2 crashes, They did not do any test, but this happened when it was placed.
When will the BQ40Z50-R2 crash,
Waiting for your reply.
Thanks
Star
Hello Star,
I'm not sure what you mean. Please clarify what they process is and what is defined as a "crash"? The BQ40Z50-R2 does not crash unless something is changed incorrectly in data flash or the schematic is not correct.
Please share schematic, .gg file, and their test conditions.
Sincerely,
Wyatt Keller
Hi Wyatt
Thanks for your reply.
The test process is as follows.
They sent 12 batteries to the customer in shutdown mode. After two months storage, they inserted the battery to their system to wakeup and charge.
6 batteries could not be waked up and exited from shutdown mode. The other 6 batteries were activated normally.
The six inactive batteries needed to disconnect the cell and reconnected the cell then powered on it can work normally.
The following are schematic and gg files.
Please give some suggestions.
Thanks
Star
Hello Star,
If power is supplied to PACK side on the PACK pin above V startup then the gauge will wakeup from shutdown. Did they confirm it work before shipping, was it unresponsive after assembly?
Sincerely,
Wyatt Keller
Hi Wyatt Keller
Thanks for your reply.
The battery can wakeup after assembling, also can wakeup from shutdown mode before shipping.
Is there anything else that may cause wakeup failure(It needed to disconnect the cell and reconnected the cell then powered on it can work normally.)
Waiting for your reply.
Thanks
Star
Hello Star,
As long as there is enough power to keep the gauge active and a voltage is applied on the PACK pin the gauge should wakeup from shutdown. What are the voltages on the gauge pins for PBI, PACK, BAT, and VCC after they try to wakeup the gauge?
Sincerely,
Wyatt Keller
Hi Wyatt Keller
Thanks for your reply.
They try to apply 16.4V on pack pin, the PACK pin voltage is 16.4V, PBI is 16.0V, BAT is 16.25V, VCC is 16.0V, cannot wakeup the gauge.
Thanks
Star
Hello Star,
If PBI is high the gauge is most likely active, it may just not be responding to commands. Can you share a scope capture of the TS1 pin, if it is pulsing at approximately 250ms this means the firmware is executing but the communication is not responding. If it is not pulsing then firmware is not executing.
Sincerely,
Wyatt Keller
Hi Wyatt Keller
Thanks for your patience.
The TS1 waveform as below:
The TS1 keep low, firmware is not executing.
Why does the firmware not executing?
Waiting for your reply.
Thanks
Star
Hello Star,
What is retuned by the gauge when you read word 0x0d?
Does the gauge respond to anything over SMBus?
Sincerely,
Wyatt Keller
Hi Wyatt
There is no response. The battery is inserted into their system, and cannot communication.
When reading with EV2400, also cannot communication.
Thanks
Star
Hello Star,
They tried communicating on both address 0x17 and 0x16 with read word 0x0d and there is no ACK?
Design team is not sure of root cause from the description given. If PMID is powered then the gauge is not in shutdown, but TS pin not pulsing indicates FW is not running. Only other options is it is in ROM mode or the firmware was corrupted, which doesn't seem to be the case if a POR fixes the issue.
Sincerely,
Wyatt Keller
Hi Wyatt
Thanks for your help.
The customer do the ESD test can simulate the same phenomenon.
They connected the battery at the output port. The air is 15K, and the contact is 8K.
Every time do an electrostatic test, they will discharge the power to the connection port. If the discharge is incomplete or the static electricity is applied for several times continuously, the chip will not active. Then all battery cells need to disconnect and reconnect again it can work normally.
Attached the SREC file
Waiting for your reply.
Thanks
Star
Hello Star,
It sounds like the boards need to be optimized further for ESD mitigation if the ESD event is causing some type of damage or bits to flip in the gauge where only a POR can recover the state.
Can you share the board layout files?
Sincerely,
Wyatt Keller
Hi Wyatt
Attached the layout picture. The layout file is encrypted they can not share.
Whether the layout issue will cause the chip not active after 2month storage?
Thanks
Star
Hello Star,
I can't see much detail but I don't see any large issues. It sounds like when being woken up the chip had an ESD event. Just sitting for 2 months should have no impact on the gauge, that's why it should be something else causing this behavior.
Sincerely,
Wyatt Keller
Hi Wyatt
Thanks for your help.
If it is caused by ESD, How to improve ESD anti-interference ability?
Thanks
Star
Hello Star,
TVS diodes close to the point of contact, shortening and preventing any trace overlap of sensitive lines (like TS inputs to the gauge). Adding small caps to the TS lines near the gauge (10nF) are some of the general guidelines we recommend.
Sincerely,
Wyatt Keller