Dear TI experts,
The circuit below is from the spec of LM5017,
My question is why the inductor in series with a resistor R8?
When should I put R8 in the design?
thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI experts,
The circuit below is from the spec of LM5017,
My question is why the inductor in series with a resistor R8?
When should I put R8 in the design?
thanks!!
Hi,
The resistor is placed for the convenience of inductor current test.
Regards,
Hongjia
Hi,
Thanks for your reply. I have three more questions...
1. The datasheet shows two ways to calculate Cr for the type3 ripple circuit, witch one should I follow 25 or 50mV? What is the meaning of them?
2. If there is no 3300pF for C6(Cr), can I use 2200 or 4400Pf to replace it? Which one you recommend?
3. Does LM5017 include soft start feature? If I want to add the soft start feature, I had to add the external circuit below, using the diode to connect Vfb and Vcc??
Best regards
Hi,
1. It should be 25mV. You can also refer to datasheet Table 7.1.
2. You can use Equation 7 in Table 7.1 for calculation. A smaller Cr will make the ripple larger and therefore benefits stable operation for COT.
3. Yes please use the external soft start circuit to realize this function.
Regards,
Hongjia