Part Number: LM5119
Other Parts Discussed in Thread: TPS54061
Hello e2e-community,
I´m using an LM5119 buck controller in interleaved mode with external supply provided by TI TPS54061 to reduce power dissipation as shown in schematics below.
Key parameters are: 48V input voltage, 24V output voltage with 10A max. load for each channel.
During testing the new hardware I noticed audible noise depending on load condition and later on voltage level of external supply voltage. So as I investigated I found that regulator sometimes skippes pulses and sometimes lengthens pulses and when this behaviour occurs in the hearable frequency range it is noticeable when next to the PCBA.

For dimensioning the circuit I followed LM5119_Quickstart Exel sheet.
LM5119_QuickStart_TI-e2e.xlsx
First measurement below shows both swiching nodes and their inductor current without load.
Second measurement shows both nodes during 10A-load. I think this behavoir is described as sub-harmonic oscillation in the LM5119 data sheet and I modfied R_RAMP-resistor and C_RAMP-capacitor which already improved the behaviour. This was very noisy and the part changes are already included in schematic and excel above.

At further testing I disabled the 10V external supply and enabled LM5119 internal regulators at VCC1 and VCC2-pins which also seemed to improve the behaviour (=less pulse length variation =less audible noise).
I proceded to modify the external supply voltage by disconnecting anodes of V1 and V3 and feeding a voltage from laboratory power supply to VCC1/2-pins.
When setting the lab supply at 10V the various puls length still occur in the hearable range, coursor for C2 at 18kHz below at 20A load.
And with the lab supply set to 8V instead of 10V the frequency is at 23.5kHz in the example below and not noticeable anymore at 20A load.
After this i decided to ask for help here in this forum.
Is there a recommended range when using an external supply voltage? In the datasheet it says for VCC pins
I still have to modify the resistor divider of 10V-regulator to set it to 8V and check it at load condition.
Thanks in advance & BR
Florian