Other Parts Discussed in Thread: TPS62912,
Hi,
I need to design ultra low noise power supply for PID controller for our university laser research. Power consumption is estimated around 12V 200 mA for MCU, op amps and ADC/DAC. Output will drive 50 ohm load +-5V.
PID controller will be powered by 12V power supply, which I need to convert to symmetric +5V and -5V.
My first idea is to convert input 12V to to 7V by low noise step down converter (TPS62912) and later use linear regultator to achieve low noise 5V.
I want to do the same with negative voltage, so low noise inverting converter and linear regulator.
I want to use TPS62912 as low noise step down with ferrite bead to reduce voltage ripple. I have few questions about designing of such power supply:
1. Is it possible to use TPS63710 with ferrite bead configuration in feedback loop as it is done on TPS62912? I am poosting picture of TPS62912 buck converter.
Could you suggest appropriate schematic with ferrite bead solution since TPS63710 ffedback loop is not externally connected?
2. According to quesiton 1, will such configuration on TPS63710 be stable?
3. Since I assume my estimated load as low, Do you recommend to additionally dummy load DC-DC converter?
4. Will dummy loading DC-DC converter reduce the noise? I am considering voltage ripples due to low load of the DC-DC converter.
4. Would it be better to dummy load DC-DC converter right after inductor or should I dummy load linear regulator?
5. Could you recommend better DC-DC converter than TPS63710 which also uses spreaded spectrum?
Best regards
Patryk