Will the BQ26220 accurately measure coulombs, with currents out of the battery in the 16 to 100uA range, but having occasional 20mS pulses of up to 300mA. The high current pulses occur over a period of 100mS when a DC motor is activated. Typically 4 times a day. Nominal battery voltage is 6 volts. Please recommend another part if better suited for this app.
Thank you.