Hi,
I am designing a POL converter using the LM25141. I have 2 questions about it, and did not find the answer in the datasheet.
1) I would like to connect the EN pin to VCC or VDDA with a pull up resistor. Is the internal LDO (VCC / VDDA) enabled when the EN pin is low at startup ?
2) What is the current capability of the VDDA pin ? I would like to connect a 10 mA LED to this pin for prototyping purposes.
Thanks in advance.