Hi,
we are planning a design with a AM3715 and the TPS65920/30. The design should provide the possibility to realize a version with AM3715CUS (800MHz) and AM3715CUS100 (1GHz).
I have found a hint that the TPS65920/30 is not suitable for OPP1G (operation point 1GHz) - i am a little bit confused about the wording of the hint which can be found here: http://processors.wiki.ti.com/index.php/AM/DM37x_Overview#AM.2FDM37x_PMIC_Comparison
"Targeted devices: all AM37x, DM37x except for OPP1G"
Is the meaning that only the DM37x(1GHz) and the TPS65920/30 are not suitable? Or is this restriction of the TPS65920/30 valid for all 1GHz-types of the AM/DM37x family?
In this case we must plan a design with TPS659-50A3/-51or -10!?
Regards
Frank