This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28064A: UCC28064

Part Number: UCC28064A
Other Parts Discussed in Thread: UCC28060, UCC28063A,

Hi Group, 

SLUA625 details LED Driver Based on UCC28060 Interleaved ACDC Single Stage Flyback.

My application is low power (25W) but limits the transformer width to 19mm.  Using an interleaved flyback design offers the advantage of using two narrow 15W transformers. 

Noting the design is from 2011 is SLUA625 still recommended as a viable solution?

Regards, 

Stuart Linzer