This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: Chemistry ID not correct

Part Number: BQ27520-G4
Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO

Customer using GPCCHEM match a ID, but the result is not correct, chem id battery it is 1200 mAh and his battery is 350mAh. Below is the upload file and report of GPCCHEM. Please check there is anything wrong with data.

1832.GPC_ChemID_Data.zip

7181.GPC_report.txt
Chemistry ID selection tool, rev=2.54		
		
Configuration used in present fit:		
ProcessingType = 2		
NumCellSeries = 1		
ElapsedTimeColumn = 0		
VoltageColumn = 1		
CurrentColumn = 2		
TemperatureColumn = 3		
		
Best chemical ID : 117	Best chemical ID max. deviation, % : 5.48	
		
		
		
Summary of all IDs with max. DOD deviation below 3%		
		
Chem ID	max DOD error, %	Max R deviation, ratio
0	0	0
		
Warning: Deviation is above recommended level. New chem ID needs to be released for this cell. Please contact your TI representative to send the cell to Dallas for characterization		
		
		
Selection of best generic ID for ROM based devices like bq274xx		
		
		
Device / Family #1		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27411-G1C: 4.35V LiCoO2	6.67
128	bq27421-G1A: 4.2V LiCoO2	10.37
3142	bq27421-G1D: 4.4V LiCoO2	10.73
312	bq27421-G1B: 4.3V LiCoO2	19.41
Best generic ID 354		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
Device / Family #2		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	6.67
1202	bq27621: (default) 4.2V LiCoO2	8.09
1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	8.3
Best generic ID 354		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
Device / Family #3		
Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
3230	bq27426: (default) 4.35V LiCoO2	6.52
1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	8.09
3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	10.73
Best generic ID 3230		
Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID.		
		
		
0636.MiscInfo.txt
ProcessingType= 2