The parametric search on TI's website indicates that the TPS629210 has a settable UVLO. However, there is nothing said specifically about it in the datasheet or the EVM users guide. There is a UVLO threshold listed in the parameters with the note "Vin rising", which sort of indicates that UVLO is not adjustable and is triggered by Vin, as does Table 8-3 in the datasheet. The only thing that indicates a settable ULVO is the recommended layout figure 11-1, which has a resistor divider on the EN pin.
Is the UVLO on this device settable by a resistor divider on the enable pin?