Hi Team,
I have started testing the UCC2894D for my application. the following circuit is connected to verify the operation
Testing steps
1. Vref voltage is coming 5.21V when VDD supply is increased from 12V to 12.7V (initially)
2. Vfb is applied 1.55V using external power supply
3. Vin is 55V also applied using external power supply
Observations:
1. At pin 8 (i,e., Rslope), we can see some waveform
2. No output at Pin 12 and 13 (OUT and AUX)
Please suggest if any modifications are required to test the IC.
Thanks
Umamaheswararao