In section 7.3.10. the formula for RENB yields unusual values for RENB.
For instance, when Vin is 12V, the formula is RENB = 110 / (12V - 1.1V) = 10.1kohms.
When working this into the 1.2V EN threshold & the 100kohm "top" resistor I estimate a typical start voltage of (1.2V/10.1K - 1.4uA)*100K + 1.2V =~ 13V
The formula doesn't appear to work - please advise. This also contradicts the recommend RENB values from table 7-3