Part Number: BQ78350-R2-DEVICE-FW
The cell I use is actually given in CHEMID and I program it to BQ78350-R2.
But, my battery pack consists of multiple of those cells connected in series and also parallel.
As far as I could understand, the CHEMID for CEDV gauges is only used for initial SoC estimation when the BMS is booted. But, CHEMID is not used for correct gauging parameters. For obtaining correct CEDV parapeters such as EMF, EDV0, EDV1 etc., I still need to log data during 6 charge-discharge cycles as explained in SLUUB45B. Am I correct?