This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ26220 overall accuracy, latency, transfer function

Other Parts Discussed in Thread: BQ27010, BQ26220

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Good Morning,

 

I am working on BMS that's requires high coulometric measurement accuracy, two battery IC monitor devices (Bq27010) and Bq26220 (21)) sould be implemented. I would like to have further information about:

 

Bq26220:

 

Relation between the output frequency (counting frequency) and input voltage developped across the sense resistor

 

How to estimate the overall accuracy of the output data (unit : microVh), including T°C gain coefficient, Integral nonlinearity, supply voltage gain coefficient,..

 

G(VFC) Charge/discharge gain Temperature = 25 C, VCC = 3.6 88 91 94 Hz/V

 

G(VCC) Supply voltage gain coefficient

 

100 mV < (V(SRP) V(SRN)) < 100 mV 0.5 %/V

G(TCO) Temperature gain coefficient 0.005 %/C

 

INL Integrated nonlinearity

 

100 mV < (V(SRP) V(SRN)) < 100 mV 0.2% 0.5%

How fast fully conversion can be performed between the initiated of the input signal conversion and the output data (coulombs couting) => VFC (voltage to frequency converter) latency (in seconds)

 

best regards

Thank you very much