This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25800-Q1: Vin 24V Vout 23V(+18V, -5V split ) 6W in Web bench

Part Number: UCC25800-Q1
Other Parts Discussed in Thread: UCC25800

Dear TI

I will use UCC25800 Parts and verify some design conditions.

[my condition]

norminal Vin 24V(14~28V)

Vout for sic gate driver 6W(+18V, -5V)

but web bench don't work my condition.

can you explain example web bench conditions or reference quide?

(i find some example 'Using the UCC25800EVM-037 2-W LLC Converter for Traction Inverter Driver Bias Power Supplies'

but it is 2W Output Power condition. it is smaller than 6W.)

Best regards, Choi