Part Number: TPS48111Q1EVM
Hello.
I have some questions regarding the EVB design:
1) What is the purpose of diodes OR'ing at the Vs input (D10 & D11)? I suppose it is done to power the component after the input voltage has been turned-off, and the output is still charged, but why it is needed? Should it prevent from some damage?
2) One of the purposes of this driver is inrush current protection by using pre-charge or/and inrush current limiting. Why, however, three capacitors of about ~50uF net capacitance have been added to the input of the inrush protection, overriding the inrush protection effect?
Sincerely,
Alex