This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5067: Reverse polarity protection

Part Number: LM5067


Hi,

We are using LM5067 for a -48V, 10A system as per the following image. Please advice me that our circuit works as expected. Main requirement is to protect the system from accidental input reversal. Added two NMOS with a single GATE signal from LM5067 to avoid reverse input polarity.

Regards,

Vivek