Hi
The customer design with BQ25792, 3S configuration, the battery voltage is 11.4V.
Change the value of the VSYSMIN (REG0x00[5:0]) register, the VSYS voltage is always 11.4V.
Read the value of VSYSMIN (REG0x00[5:0]) 1A, write 1E, and return to 1A in about 10 seconds.
If the value of REG09_Termination_Control Register is set to 25, it will automatically restore to 05.
How to set the system voltage to stable at 12V? Does the chip have this function? Can VSYS be adjusted?
Waiting for your reply.
Thanks
Star