This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5034: Requirement of Design calculations for LM5034

Part Number: LM5034
Other Parts Discussed in Thread: UCC2897A

Hi Team,

For the following design specifications for my customer, I have suggested this part No. : LM5034

Input Voltage range, Vin = 40 to 62 V

Output Voltage, Vo = 14.5 V

Load Current = 20 A

Output Power Po = 300 W

Isolated DC-DC

Now, they want to have design calculations for this part, so could you please help me with this ASAP, and if you have any alternative part to suggest having design calculations available, please let me know.

Thanks!