I am using TPS73001 in my circuit to generate a 3v power.
below are the usage conditions
IN = EN = 3.3V
R1 = 1.6K
R2 = 1.13K
CNR = 10nF
Cout = 2.2uF
Cff = 471pF
I was expecting output around 3V but getting 2.81V and when I measure Vfb voltage it was around 1.16V and it is less than min internal reference voltage mentioned in datasheet.
i think because of decrease in vfb causing output voltage to decrease.
can anyone tell me what causing Vfb to decrease?
Regards
Arvinda