This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2807-2: Start threshold Max is same as Absolute Maximum Supply Voltage

Part Number: UCC2807-2

Hi experts

From the datasheet, the Max value for the Start Threshold is 13.5V. This is the same voltage listed as the Absolute Maximum Supply Voltage for the part.

How can we guarantee we start up the device correctly, without applying a voltage that is at or above the Absolute Maximum Supply Voltage, and potentially damaging the part?

Thanks,

Jim B

  • Hi,

    In typical applications, you can tie a resistor (startup) from VDD to the Vin and a capacitor from VDD to GND for startup. So the capacitor will be charged up and when VDD voltage reaches up to 13.5V, the IC will start to work. For VDD current, the startup current (max 0.25mA) and the normal operation current (max 2.1mA), so right after startup, the VDD voltage will drop and < 13.5V if you design the startup resistor with 0.25mA or so due to a much higher current will present right after startup. Your aux biasing voltage can be designed between 9V and 12.5V to leave some room from 13.5V.