Other Parts Discussed in Thread: UC1825
Hi,
I am looking at a design that uses the Vref to power other circuits on the card. It is used to power an LDO and as the collector voltage of a couple of transistors. The data sheet says that Vref will supply at min. 15mA. This device is being used in a military application and so, my first question is has this part been built with MIL-STD-1547 compliance? If not, then this 15mA will need to be derated in accordance with MIL-STD-1547. I am also wondering, if Vref has been designed to be 0 volts, during under voltage operation or is this voltage basically uncontrolled during under voltage operation? Also, there seems to be 1.1uF capacitance across it to ground. The data sheet states there should be 0.1uF. Is there a performance impact to increasing the capacitance? Do you recommend using Vref to power other circuits? What is the intended use for Vref. Is it intended to be used with the UC1825 only?
Thanks!
Susan