This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23521: Question about recovery , inrush current

Part Number: TPS23521


Hi

 1. The OCP operates and recovery only when the load current reaches 0A.
Can I adjust the recovery point?
For example, if the load falls below 1A, it is a recovery.

2. Sometimes, when turned on even under a very small load, it is recognized as an inrush current and cannot operate.
Can I adjust the inrush limit point?

Thanks