Other Parts Discussed in Thread: BQ25306,
Hello,
I am using the 3.8V 385mAH battery with the Bq27z561-r2 module. I'm also using the Bq25306 module to charge the battery.
These are the parameters I have set as the learning cycle document and the battery datasheet.
In this case, full charge is not occurring(FC bit not set). Charge term taper current, Quit current and Charge current threshold is set below 38mA. And the charging was stopped at the 60mA.
Is the charger IC(BQ25306) capable of providing 35mA(C/10) current?
I am sharing the log file of the learning cycle.
Please let me know if any changes are require in parameter setting. Or do I need to change the charger module?