Hi Experts,
In order to start UCC28740, should both VDD pin and HV be connected? If yes, what should the minimum value of V(hv) be? Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
In order to start UCC28740, should both VDD pin and HV be connected? If yes, what should the minimum value of V(hv) be? Thank you!
Hi Skylar,
Thank you for the query on UCC28740.
In short, yes both VDD and HV have to be connected. Minimum recommended voltage at HV pin to have reliable startup is atleast 30V.
Regards,
Harish
Hi Harish,
Thanks for your prompt reply! There is a another question about the datasheet. The bias-supply operating voltage of VDD is from 9V-35V but VDD turnon threshold is 21V. I wonder that if VDD=18V and V(HV)=390VDC, will UCC28740 start up? Thank you!
Regards,
Skylar
Hi Skylar,
Thank you for the query.
There should be no concerns to start up ucc28740 at the above conditions. VDD will cycle between turn on threshold of 21V and 8V during HV startup and fault conditions. But once the auxiliary winding is up, that voltage must lie between 8-35V for normal operation. Please let me know if you have additional questions.
Regards,
Harish