This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck Converter Wide Input Range Input:(20V-96V) Output (5V/~2.5A)

Other Parts Discussed in Thread: LM5012, LM5013

Hello,

I'm searchimg for an Buck-Converter. I have an Applicationwith following parameters:

Input Voltage: Will be between 20V- 96V

Output Voltage: 5V.

Current: 1.5A at 5V - Peak will be around 2,5A.


Important is that the DC/DC Regulator can handle the wide Range of different voltages. Can you recommend any DC/DC regulator?


Best regards

Fabian