Part Number: BQ27426EVM-738
I am doing the automated learning cycle. Battery capacity is 3500mAh, with a float voltage of 4.35V.
After 22 hours of the learning cycle, the BQ Studios GUI is showing 99% and won't move on to the next step. The power supply shows 4.35V, the GUI shows 4.35V, and the current is well under the termination current (its 1mA).
I tried changing the Data Memory > Chem Info > Taper voltage to 4.34V and also changed the V at chg term to 4.34V.
Does this have something to do with the FC bit? I thought the FC bit was enabled by default?
(I also filled out the parameter Q&A. Taper rate is the default 100)