This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65982: USB not detected by PC

Part Number: TPS65982
Other Parts Discussed in Thread: OMAPL138, , TPS65987

Hi,

I am working on the USB-C PD controller TPS65982 to add USB-C connector to our product, I am using OMAPL138 as the processor for the product.

I have connected the OMAPL138's USB0_DP and USB0_DN to TPS65982's USB_RP_P and USB0_RP_N respective. When I connect the device to PC its shown under "libusb-win32 devices" as TPS65982 even when I am running USB2.0 application on the device.

If I connect the device via usb-b to PC it is shown under Other device -> Generic Bulk Device , this what we are exposing device as. Why is it detected differently when connected using USB-C ?

The PD controller is configured to act as Dual Role Port using the standard config provided in Application Customization tool. 

Is there something I am missing?

Thanks,

Kushal