Hi,
Is the switching pin of the LM5163-Q1 (SW) in high impedance for disabled power supply? (EN < 1.1V)
Thank you,
Antonio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is the switching pin of the LM5163-Q1 (SW) in high impedance for disabled power supply? (EN < 1.1V)
Thank you,
Antonio
Hi Antonio,
Thank you for posting! I believe it will be high impedance when disabled. However, in a real circuit the power inductor still offers a path to Vout.
If you want the SW to be high impedance right away when pulling EN low, it may not be the case because the internal VDD may still hold the voltage to enable the low side FET. The FET will be turn off after the VDD decays, so there will be some delay time which is not given in the datasheet.
Thanks,
Youhao
Thank you
Therefore, if EN of the LM516x is always kept low (or if an unspecified delay is expected),
there shouldn't be any problems feeding Vout from another regulator/power supply (SW is in high impedance).
Thanks again,
Antonio
Hi Antonio,
Let me double check with our designer (ooo currently) to be 100% sure that there is no weak pulldown implemented when the device is OFF.
By the way, feeding Vout higher than the VIN will be a problem. Note that the high side FET has a body diode :-)
Will update next week.
Best Regards
Youhao
Hi Antonio,
Sorry for the delay. I got the confirmation from our design team that the SW pin will be in high impedance when EN is <1.1V.
Please do not forget the other conditions that we already discussed: residual VCC voltage may keep the low side FET on before it decays; and the high body diode can provide a low impedance path to VIN.
Thanks,
Youhao