Hi all,
I am working on switching from SPI to I2C and am running into a few interesting errors. I am using the same RAM settings that have been in production, the same schematic that hasn't changed for 6+ months, just only switching from a SPI based BQ driver to I2C.
I sent our command to close the FETs and I noticed the Discharge FET was opening up after about 6 seconds. There are no faults, no safety alerts, the device is unable to enter sleep, it is at nominal conditions, and no current. The charge FET stays closed, but the Discharge FET opens up. Is there any reason that this could happen? The DDSG pin is asserted after 6 seconds which means the chip thinks it shouldn't be allowed to close the FET.
Thanks,
Kyle Garland