Other Parts Discussed in Thread: TPS7A30, TPS7A49
Hi Team,
Can you please help with the inquiry below?
In the datasheet, the enable pin has a maximum rating of +36V to VIN or +36 / -36 V to GND. In the electrical characteristics, it specify +15V in the max value, with a -1V out. If the TPS7A3001 is supplied with a -33V, it is ok if the enable pin is supplied with a +16V through a 16k resistor?