Other Parts Discussed in Thread: TPS25750,
Hi Team,
Our customer use TPS25750+BQ25792.
If Input source power is lack(For example, 5V/3A etc.), BQ25792 can’t charge to battery so IBAT=0mA(Supplying only to SYS).
Then, STAT pin is Low.
Even if IBAT=0mA, STAT pin is Low.
Is it correct behavior?
By the way, I have already confirmed “Table 9-11. STAT Pin State”.
I guess that BQ25792 doesn’t reach “Charging complete” so “STAT pin is Low” is correct behavior.
Regards,
Hide