This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38691-Q1: P/N Clarification

Part Number: LP38691-Q1
Other Parts Discussed in Thread: LP38691

Hi TI expert,

May I know whether I can directly replace LP38691SD-5.0/NOPB with LP38691QSDX-5.0/NOPB?

And how to identify whether LP38691QSDX-5.0/NOPB is qualified as AEC-Q100?

Or all solution with WSON package are qualified as AEC-Q100?

Looking forward to your reply,

Thank you.

  • Hi Chia,

    Yes, you can directly replace LP38691SD-5.0/NOPB  with LP38691QSDX-5.0/NOPB. 

    LP38691QSDX-5.0/NOPB is AEC-Q100 (automotive) qualified. Parts that are automotive qualified usually have -Q1 suffix after the GPN. 'Automotive' is also included in both the product description and the first page of the datasheet. 

    I hope this is helpful,

    Erin