This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: vout drops much @ ~20mA Iout

Part Number: TL431


Hi Team, 

my customer use TL431B to generate a regulated voltage as driver for high-side FET in half-bridge.  circuit as below ( see black) 

If no load, Vout is stable as 17.9V, but if adding the MOS ( that is , adding ~20mA), Vout drops much to ~15V.  But if using p2p device from other vendors, it is always stable.  Since the Vout/Vin has floating GND reference ( Source of FET is high voltage ) , I suspect it is related with common mode voltage.  

Also, we found adding a 1nf cap in parallel with the 1kohm ( as shown in RED) , then no such issue. 

Could you please kindly add your comments on this? Thanks. 

BRs

Given