Other Parts Discussed in Thread: LMZ34202
I am considering using the TPSM63602 buck converter in a system to generate 16V output based on a 36V input voltage. The TPSM6302 is rated for an input voltage range of 3V to 36V so my application would come in at the upper spec of this buck converter. The absolute maximum voltage for this converter is specified as 40V.
I would tend to look for another buck converter with a wider input range so I'm not operating this device at the maximum specification, but what is the actual guideline for selecting an input voltage range? What is a good input range margin to consider since technically this buck converter 'could' work for my purpose?
The datasheet, page 14 is stating: "The device is intended for step-down conversions from 5V, 12V and 24V supply rails". Then page 15 of the datasheet is stating: "The TPSM63602 module is intended for step-down conversions from typical 12V, 24V and 28V supply rails. So is the 24 (or 28V?) the intended input range for this converter?
Best,
Peter