Part Number: TPS717

Vin max +0.3V = Ven = 7V?
max Ven 7V
Vin is designed for 3.3V and Ven is 5Ven.
Now, the system is working well.
I would like to see if there is no problem with the system operation.
Can I use it like this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS717

Vin max +0.3V = Ven = 7V?
max Ven 7V
Vin is designed for 3.3V and Ven is 5Ven.
Now, the system is working well.
I would like to see if there is no problem with the system operation.
Can I use it like this?
Hi Taehun,
For your application Ven = 5V should work fine as per the datasheet notes.

Regards,
Andres