This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS717: I Use 3.3 Vin. I want to know the range of VEN usage.

Part Number: TPS717


Vin max  +0.3V =  Ven = 7V?

max Ven 7V

Vin is designed for 3.3V and Ven is 5Ven.

Now, the system is working well. 

I would like to see if there is no problem with the system operation.

Can I use it like this?