This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: BQ34Z100PWR-G1

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100

Hi,
I need schematic review designed based on BQ34Z100PWR-G1. I also have following question regarding design.

  1. The load/charger should connect with BAT+ and pack - points. In my case, the load will be internal circuitry on the board i.e. 5V regulator etc. I am confused about the GND point that either i should connect GND of other circuit with BAT- or Pack - point. I believe it should connect with pack - assuming all these circuits as load.

Thanks