Hi all,
In case of using the BQ25122 in stand alone mode, If i connect ILIM, ISET and IPRETERM to GND, what will be charge current and the input current limit?
what about the precharge current, what will be the % of ISET?
Thanks
Regards,
Damien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
In case of using the BQ25122 in stand alone mode, If i connect ILIM, ISET and IPRETERM to GND, what will be charge current and the input current limit?
what about the precharge current, what will be the % of ISET?
Thanks
Regards,
Damien
Hi Damien,
When the ILIM, ISET, or IPRETERM resistors are tied to GND, default register values are used for the configured values. For the BQ25122, the default register values will be:
- ICHG = 11 mA
- ILIM = 50 mA
- IPRETERM = 0.5 mA
In this case PreCharge current is not expressed as a % of ISET.
Best Regards,
Juan Ospina