Other Parts Discussed in Thread: EV2400
Hi TI Teams,
We are intend to use BQ35100 to measure the battery capacity which based on a 550mAh Li-lon battery, with the operating currents of (7~30uA) and (100~300uA) respectively. Can u help to confirm whether this fuel gauge is suitable? If not, can u gave us some bettery suggestion for our application?
In addition, we also want to confirm that does chem id setting require a special adapter like EV2300 or EV2400? Or can we use the I2C of MCU to set it directly?
Thanks,
Kind Regards