Hello, I have used this support before for TI parts simulated in TINA but this is an IGBT that TINA is having difficulty accepting the netlist I provided. The netlist is in *.LIB file format, TINA would not accept that - it indicated the following - 'More than one subcircuits or models found in this file. Select the one you need from the list.' Which I did and produced a text file from it. TINA accepted that to a point then would not proceed to fully finish the model.
Here are the details:-
Component - Infineon Reverse Conducting IGBT - IKN01N60RC2
Netlist text file - IKN01N60RC2.txt
Details of Netlist - .
SUBCKT IKD04N60RC2_L1 C G E PARAMS: TJ= {TEMP}
X0P3N E C Z04G6 PARAMS: TJ= {TJ}
X0PBD C G E Z00DY PARAMS: TJ= {TJ} N4OW9=0.0107
+N4QOS=130 N4SW8=-1.5
+N4WN5=0.105E-9 N4XNG=7 N4Y3T=3.25E-8 N4Z0X=0.45E-10 N527G=1 N562D=15E-09 N56WE=1.00000E-10
+N595B=1E-3 N5BY0=1E-6
+N5CQA= {1.4E-8} N5DOJ= {6E-9/0.0107} N5HBQ=3E-10
.ENDS

The pic above can't be made clearer but hopefully you get the picture! The error message is 'Undefined subcircuit Z04G6. (C:\Program Files (x86)\DesignSoft\Tina 9 - TI\EXAMPLES\SPICE\TSPICE.LIB)
So then I click 'OK' and it comes up with another error message, which is 'The circuit cannot be opened or cannot be converted to a macro.'
This has happened before and is not a rare event! I do have some mosfets I need to model in the same circuit but it is likely that I will need help for these too!
Thanks for any assistance from anybody.
Best regards,
Peter J Partridge