Hi, We are facing problem in cell measurement in BQ76952 AFE design. First cell drops to 1500mV(approx) randomly when battery is idle. Balancing is also not happening at that time. The nearby cell voltage is also ok. These are the cell voltages at that time. This remains only for 3 to 6 seconds only. Please suggest solution.
1310 | 3413 | 3415 | 3410 | 3412 | 3411 | 3413 | 3411 | 3412 | 3412 | 3414 | 3409 | 3414 | 3411 | 3411 |
Thanks and Regads
Sunil Kumar