Other Parts Discussed in Thread: GPCRB
Hi Team,
The customer programmed 2 fuel gauges with the same configuration, the cell voltage is 3.9V, and the RSOC is 50%.
- One of the battery packs is in relax state, and the ambient temperature is cooled to -20°, and the RSOC of this battery pack is gradually reduced from 50% to 18%. See the LOG data and GG file below; the current set parameters are RELAX_SMOOTH_OK=1, RELAX_JUMP_OK=0, why is it still jumping?
NT02_GPCRB_7105_20230301bq27z561R2.gg.csv
NT02_minus20degC_simulation_20230317.log
- The other battery pack was charged to 100% at room temperature and left to stand, and then the ambient temperature was lowered to -20°. The RSOC of this battery pack did not jump during the cooling process; why is this?
Regards,
Hailiang