Other Parts Discussed in Thread: TLVM13620
I'm currently using a TL2575 for a application with the following values:
Vin = 24V
Vout = 5V
Peak Iout = 750mA
I have a 100uF input capacitor, 330uF output capacitor and 330uH inductor.
Is the inductor properly sized for the load that I'm drawing?