Hi expert,
I check the reference circuit and always find a resistor like 10k or 121k from TSEN to GND, could I remove it?
If not, why do we add it here?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
I check the reference circuit and always find a resistor like 10k or 121k from TSEN to GND, could I remove it?
If not, why do we add it here?
Hello,
TSEN should be around 0.8 V and will be pulled high to 3.3 V by controller if there is an issue with temperature, which needs the resistor there. If the resistor is not there, then the signal would be left floating. I would not remove the resistor.
Best,
Ryan