Hi
I have a query need your help.
AOLD is set to 0XF4, RSNS=0, Rsense is designed to be 1mΩ (CC Gain and Capacity Gain are both 1.415mOhm after calibration).
Overload current = –27.76 mV / 1.415 mΩ = 19.6A, the Safety Status AOLD will only be triggered when Current() > 19.6A.
But when the Safety Status AOLD is triggered, it is found that the Max Load Current is only 14A, 15A.
Does it normal?
What is different with Max Dsg Current and Max Load Current? AOLD current will update in Max Dsg Current or Max Load Current?
Waiting for your reply.
Thanks
Star