Other Parts Discussed in Thread: BQ25720
Hi team,
My customer is designing BQ24770 and asked following questions regarding system voltage in NVDC. Could you help answer this questions?
1. Could you confirm if it is a normal behavior that the system voltage is ~200mV above than the battery voltage when BATFET is off(Charging disabled)?
Please refer to below customer's charging profile. Also, from what I found in BQ25720's datasheet, there's a comment that it is normally 150mV above than the battery voltage.
2. What is the value for the BQ24770 then? I couldn't find in the datasheet.
3. If you don't mind, Could you please explain why there is a voltage difference when the charging is done?
BQ25720 datasheet comment:
Thanks,
Jay