Other Parts Discussed in Thread: BQSTUDIO
Hi
The customer test with BQ25798EVM, they find these 2 registers are affected by the input power.
Test condition as below:
The charging power supply is 15V-300mA, the ambient temperature is 24 degrees.
1, Fully discharge the battery, from the bqstudio software, the value of REG05_Input_Voltage_Limit Register is 7100mV, and the value of REG06_Input_Current_Limit is 1010mA.
2, Modify the REG05_Input_Voltage_Limit Register to 22000mV, and the value of REG06_Input_Current_Limit to 3000mA.
3, REG05 is set successfully, and the REG05_Input_Voltage_Limit Register becomes 22000mV, but REG06_Input_Current_Limit is still 1010mA. The weirdest thing is that the power supply charges the battery at 15V - 0.007mA.
the register as below:
* Created: Wed Mar 29 12:00:07 CST 2023
*
* Format: Register Name tab Character,\t Register Address tab Character,\t Hexadecimal register value.
* Device: BQ25798
* BQZ Container: Charger_2_00-bq25798.bqz
*
REG00 14
REG01 05AA
REG03 00C8
REG05 28
REG06 002C
REG08 32
REG09 01
REG0A E3
REG0B 00DC
REG0D 4B
REG0E FD
REG0F A2
REG10 80
REG11 00
REG12 00
REG13 85
REG14 1E
REG15 AA
REG16 C0
REG17 7A
REG18 54
REG19 002C
REG1B 4D
REG1C 70
REG1D 01
REG1E C0
REG1F 00
REG20 00
REG21 00
REG22 00
REG23 00
REG24 00
REG25 00
REG26 00
REG27 00
REG28 00
REG29 00
REG2A 00
REG2B 00
REG2C 00
REG2D 00
REG2E B0
REG2F 00
REG30 00
REG31 009C
REG33 0013
REG35 0FA6
REG37 0000
REG37 0FC6
REG3B 3406
REG3D 3422
REG3F 0253
REG41 0026
REG43 0000
REG45 0000
REG47 00
REG48 19
Another question, when EN_ICO is disabled, and the ILIM_HIZ pin is set to 1.5A, but the REG19_ICO_Current_Limit value returns 500mA, why not 1.5A?
Waiting for your reply.
Thanks
Star