hi,
need you check if the default value of REG00[BIT6] is 1 or 0. seems there is a conflict in BQ25890H datasheet.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ken,
I have double checked and the default value of REG00 bit 6 is 1b (enable ILIM pin). We will work to fix the conflict in figure 26 in the datasheet. Thank you for pointing this out.
Best Regards,
Garrett